This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can I increase the range of Bluetooth without decreasing speed of transferring data?

Hello Everyone,

I have an Issue related to Bluetooth. I want to Increase the range of Bluetooth for sharing data between multiple devices without decreasing the speed of transferring the data. If it is possible then kindly give me a solution of it. I will really appreciate those one who can help me in this regard.

Thanks In Advance.

Regards: Michel John

  • Hi,

    Have you considered the following?

    - increase the Tx Power

    - if not already done, use "connection" mode rather than "connectionless" mode 

    - use coded PHY - potentially reduce the connection interval, increase the MTU and the number of packets per connection interval in order to keep the same througput

    - chose antennas with a better attenuation

    - select channels with less interference

    - work on the design of the product to reduce the interference / attenuation caused by the user

    I hope this will help,

    Regards,