Part Number: CC2564MODA
Hi,
We make an intelligent rocker product with the CC2564MODA, which is matched with STM32F407VE.
After burning FW, according to the datasheet, the normal power on sequence should be as follows:

but our board RTS is always low level and there is no change process of H - > L.
what may lead to this problem?
And CTS is abnormal,The voltage at terminal A of shift IC is 1.8V, terminal B is 0V:

The hardware refers to the public circuit.The measured voltage and 32.768KHz clock signal are normal.UART_RX is high,UART_TX is low.
The attached file is the circuit diagram for your reference.
Look forward to your reply!
Lisa