Part Number: CC2564MODA
Other Parts Discussed in Thread: TLV320AIC3254, , CC2564C
Goodmorning
we are developing a BR / EDR bluetooth system with full duplex audio and custom cards made by us that have the following components: CC2564MODA + MSP432P401R + TLV320AIC3254 + Bluetopia 4.0.3 + BT Service Pack v1.8 (like the Launchpad combo system) .
Currently we have implemented the FW which is based on L2CAP and ESCO and we have got a working solution(WideBand assisted, audio is routed via I2S).
In the open field and with static devices, communication seems to be optimal even at great distances (~ 70 meters).
While moving the devices and also a shorter distances, we encounter a leak that we are not able to detect via firmware. It is particularly noticeable when there are walls or objects between the devices.
We also notice the same behavior with the launchpad system with the example SW HFP AG and HFP HF.
Our goal is to achieve always clean full duplex audio communication between devices at a distance of at least 15 meters with devices in motion and through obstacles such as walls or car doors. Would it be possible to get it with this configuration?
Where to intervene to achieve what we need (at the firmware level in particular)?
If more information is needed, I am at your complete disposal, but i would rather not share detailed information publicly.
Thanks in advance
Alessandro