Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650
Hello Everyone,
We have an application which has to be developed on CC2650moda .
I am using the SPPclient and SPP server Code to develop my application.
I have dumped SPPclient firmware in one CC2650mod and SPPserver firmware in another CC2650mod.
I am able to Connect the SPPClient which acts as Central to SPP server which acts as peripheral and able to communicate via UART Serial terminals from either side.
and also when the SPPclient(Central) is disconnected from the SPPserver(Peripheral) i am even able to connect the SPPserver(Peripheral) to Mobile phone where i can communicate from there with it.
But can i connect it to multiple Mobile phones at same time is my question?
I need to use the sppclient app server firmware for my development as it suits my application....how to add this above feature to this firmware?
Regards
Sanath Rai