Other Parts Discussed in Thread: CC2650
Hi E2E,
Is there a proper orientation required for the device to use the accelerometer properly? When the customer is using the device where the device logo on the accelerometer is facing up, all z-axis measurements are negative. When the logo on the accelerometer is facing down, all the z-axis measurements are positive. Also, when the sensortag is connected to the app, according to the customer, the z-value seems to read properly for a couple seconds, and then the reading displays as 4.0 or -4.0 consistently for a longer period of time. Is the accelerometer working properly? Is calibration for the accelerometer needed and how they can do this?
Here are some screenshots. The sensortag was at rest on the table.

Regards,
Carlo