Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650
Hi,
I am trying a create a custom simple peripheral project from example simple peripheral project available in ble_SDK_2_02_06_07 for CC2650 launchpad. Later, I want convert this code to support CC2650MODA. When I am trying to add any files to the code, it is showing that cannot add files in the virtual folder.
My question is that is there any simple peripheral project available for cc2650lp or cc2650MODA which can be editable or how can i convert the project in the virtual folder to local folder.
Basically I want to create a custom project using simple peripheral project for CC2650MODA. Am I going in the right direction?