Part Number: CC2564C
Hi, there:
I am using CC256xCOFN-EM + CC256xEM-STADAPT with HCI tester. (connected to Windows through a FDTI connector)
with below connection
CC_UART_TX <--------> FTDI CONN's RX
CC_UART_RX <--------> FTDI CONN's TX
CC_UART_CTS <--------> FTDI CONN's RTS
CC_UART_RTS <--------> FTDI CONN's CTS
CC_VCC <--------> 3.3V
When sending excuting HCI commands, it always reported "timeout error" as below:
12:59:05.914 ERROR - Timeout waiting for event HCI_Command_Complete_VS_Start_VS_Lock_Event
12:59:05.914 ERRORed Line (11): Wait_HCI_Command_Complete_VS_Start_VS_Lock_Event 5000, 0x00, 0xfe37, 0x00

My HCI port setting as below:

Please help me do a kind check on this issue?