This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Unusual high current consumption

Part Number: CC2650
Other Parts Discussed in Thread: CC2640, CC2640R2F

Recently we discovered an increased current consumption in the latest production batch of our application. Between BLE advertisement intervals the MCU goes to sleep and normal current consumption is around 3-8µA. However the new production shows the idle current consumption is increased to 35-80µA.

Some background information:

  • The application is advertising every 1800ms a BLE packet
  • 2 layer PCB design, 1.6mm thickness, FR4
  • Both layers do have ground plain
  • Only a button connected and a boost converter for driving blue LED
  • Powered from a CR2032 battery
  • Exact part number: CC2650F128RHB

We tested following:

  • Multiple 32kHz crystals -> no solution
  • Different load capacitor values for 32kHz crystal -> no solution
  • Resoldering all CC2650 connections with only flux -> temporarily resolves the issue. Current drop to 3-8µA but after a couple of days this effect is gone
  • Resoldering the X32K Q1 and Q2 pads with flux  -> temporarily resolves the issue. Current drop to 3-8µA but after a couple of days this effect is gone
  • Different solder paste in production (ON338CPP and WS820) -> no difference
  • Washing the PCBs -> no solution
  • Removing the buck converter -> no solution
  • Matching the 2.4GHz antenna -> no solution
  • Adding some coating on 32kHz crystal pins of MCU (for example SL 1307 FLZ-HT and silicon coating) -> temporarily resolves the issue

We are out of possible solutions and have 4000 problematic PCB at our customers.

Are there any thoughts or solutions?