Part Number: CC2642R
Hello, I have a quick question about utilizing I2C:
Is it possible to have two I2C ports running in parallel, with one being accessed by Sensor Controller and the other being accessed by the main CPU?
Thanks for the help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2642R
Hello, I have a quick question about utilizing I2C:
Is it possible to have two I2C ports running in parallel, with one being accessed by Sensor Controller and the other being accessed by the main CPU?
Thanks for the help!
James,
I'm sorry, but according to the CC2642R datasheet and the reference manual, there is only one I2C module available on this device, I2C0. This means that only one I2C "port" can be used by either the Sensor Controller or the main CPU.
I hope this helps.
-Luis
You are correct. After a second look, the Sensor Controller is capable of I2C communication independent from the I2C0 module. In this sense, yes, they can run in parallel. I'm sorry for the confusion.
-Luis