Part Number: CC2652R
Other Parts Discussed in Thread: SYSCONFIG
Hi,
An early "sorry" if I missed it in the BLE Mesh documentation.
I'm trying to figure out of it is practically possible to add an additional advertisement set to a BLE Mesh application setup as "Mesh + Peripheral"?
The reason I'm asking is because it seems that the "default" advertisement set is forced to be "Extended" type, which is an issue in my case. The use-case I'm looking at need to also support legacy advertisement for the "peripheral half" of the application. Is this possible to achieve today? Is it a SysConfig limitation (as it wont allow it) or does it relate to the mesh layer?
Some additional info:
I'm using the latest CCS installation and the 5.20 SDK.
Best regards,
Max