This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564C: Does the CC2564C chip allow an MTU size larger than the standard size when connecting via BLE

Part Number: CC2564C


Does the CC2564C chip allow an MTU size larger than the standard size when connecting via BLE? We are working on a new device that will connect to one of our tablet devices employing the TI CC2564C chip. The new device is BLE only and we would prefer to transmit using a larger MTU size. We looked at the data sheet and they tell us a larger MTU is available for standard Bluetooth but it is not clear if an MTU larger than 23 bytes is available when using a BLE connection

Thanks