Trying to calculate and to simulate antenna's matching network (between RF_N,RF_P and antenna) I'm little bit confused with a results that I've got.
I'll very appreciate you if you'll explain or give me some hints to understand this network.
Looking at this network I've divided it onto single ended and differential matching networks.
The single ended network is comprised from L252,C253 and L253 parts. All references according to the Figure 20 of CC2540 data sheet.
The differential to single ended network is comprised from L251,C252,L261 and C262 assuming that C251 and C261 are decoupling.
When looking at the single ended matching network and assuming that antenna impedance is 50Ohm I've got single ended impedance looking into L252 in a region of 73.8-j21.
So from now balun which is built up from L251,C252,L261 and C262 should match RF_N and RF_P output differential impedance to the single ended source that is 73.8-j21. Differential output Impedance according to the data sheet is 70-j30 (the data sheet
defines an optimal load as 70+j30 and I suppose that the differential load for optimal matching is 70-j30).
As I know when calculating balun the following equations are used:
L=Rinner/(2pi* F)
C=1/(2pi*F *Rinner)
Where F is a resonance frequency (2440 MHz)
Rdif -- output port differential impedance
Rse – single ended port impedance
Rinner = sqrt (Rdif *Rse) and it's a inner impedance with a only real part
So, in my case Rdif=70-j30, Rse=73.8-j21 and Rinner is a complex number.
Also when I calculates balun resonance frequency as F=1/2pi*(sqrt(L*C)) with data sheet values I'm getting F=3.56 GHz (L=2nH and C=1pF)
So I cannot see here any matching and I'll very appreciate you if you give me some hints and point out on my mistakes.
If you have any reference or application notes I'd like to get it if it possible.