Other Parts Discussed in Thread: CC256XCQFN-EM, BOOST-CCEMADAPTER, CC3200, CC2564C
My setup:
CC256XCQFN-EM
MSP432P401R launchpad
BOOST-CCEMADAPTER
CC3200 AudBoost
Code Composer Studio Version: 10.4.0.00006
BT Stack: CC2564CMSP432BTBLESW-v4.2.1.1 (I would really like to use 5.0 or greater Stack)
My Questions:
1)
I would like to send an event data just like mentioned below but the data is the custom one for our use case only through HFP?
The below example perfectly works for us.
eg. "AT+XEVENT=HELLOFROMHFP, 1\r" which API should I use for this one in bluetopia stack?
Mic / Headset will send the PTT commands via HFP link as follows: PTT press down send out: "AT+XEVENT=TALK,1\r" PTT release send out: "AT+XEVENT=TALK,0\r"
This is mentioned as in (Bluetooth SIG HFP1.6 Documents as shown) below!

how can I achieve this above functionality in TI CC2564C on its default TI(i think it's bluetopia) stack?
2)
Also regarding the BT certifications for my setup what will it be in the end? BT 4.2 or BT5.1 ?? as in this below link
https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1021860/cc2564cstbtblesw-cc2564c/3776991?tisearch=e2e-sitesearch&keymatch=bluetopia%2520CC2564C#3776991
3)
My use case is Embedded No-os Target (can use FreeRtos on STM32 if required) Is there any other stack available apart from Bluetopia which is reliable?
Is there a 5.1 version of Bluetopia coming soon if so when is it getting released ?
Thanks in advance.