This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Does the OAD function conflict with the external flash used in the sensor controller?

Part Number: CC2640R2F

In the design of one of my projects, I want to use the external flash in the sensor controller to operate, because I want to operate another device of the SPI bus, so I simply put the external flash in the sensor controller for operation. But now i am worried t hat if the OAD function of the chip is used, can the read and write operations of the external flash no longer be put into the sensor controller?