Hi team,

For transmission intervals less than the connection interval, if the transmit interval (SimpleProfile_SetParameter(SIMPLENFILE_CHAR5, SIMPLENFILE_CHAR5_LEN, charValue5) is set to 36 ms, the connection interval is set to 37.5, As shown in the red section.
After multiple connection events, there are two transmit events before the connection interval. So do these two transmit events go out on one connection event? Does APP_SUGGESTED_PDU_SIZE need to set up twice the byte of the data PDU at a time? (customer believes the PDU size should be the same as the number of transmitted data to reduce power consumption) Or will it be sent on the next connection event in turn? So there's a lot of latency for a long time.
Could you help check this case? Thanks.
Best Regards,
Cherry