Other Parts Discussed in Thread: CC2540
Is it possible to connect a USB connector in a self powered mode to the CC2540 ?
Are any GPIO pins (except the dedicated USB pins) needed ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2540
Is it possible to connect a USB connector in a self powered mode to the CC2540 ?
Are any GPIO pins (except the dedicated USB pins) needed ?
Thanks.
The CC2540 has a USB module.
In the usb dobgle board, the power to the board is supplied from the USB bus - it is called bus powered.
I want to create a design in which the power to the CC2540 is supplied by another source, and the USB is used only for communication (It is called self powered).
Thanks,
Sasha.
This is an interesting question, I would love to have an answer to this too. Also how much current is drained trough the DVDD_USB pin? I have to option to power DVDD_USB from VBUS, but then I need a 5 to 3V converter which will add cost. If I power it directly from the battery, it will obviously add a load to the battery therefore shorten it's life. Also in self powered mode do I need to monitor the VBUS? I think the USB specification requires this, but I'm not sure.
If I power DVDD_USB from VBUS, what happens if my battery is empty (VBUS is higher than VDD)? Could this in any way damage the chip? Is there a safe operating area, say battery goes down to 2V and VBUS is still 3.3V?
Thanks
Reto