Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650
Hello,
I am using
CCS7.4
Compiler TI V5.2.4
BLE SDK Version ble_sdk_2_02_07_06
Example "Simple BLE Peripheral"
BLE SCANNER app is used to transmit data from android to CC2650
I have modified code as per said by "YK" from this website "sunmaysky.blogspot.com/.../add-write-capability-to-characteristics.html
Then I done following changes
#define SIMPLEPROFILE_CHAR5_LEN 50
I can write 20 Byte from BLE scanner to CC2650 successfully.
BUT when I transmit more than 20 byte the array
simpleProfileChar5[SIMPLEPROFILE_CHAR5_LEN] is overwritten.
NOW THE PROBLEM IS:
When I send alphabets for example data, abcdefghijklmnopqrst, which is stored as 0 to 19 array index that is 20 byte and I get this response where 20 byte are received properly.
as shown in image

But, when I send abcdefghijklmnopqrstuvwxyz which is 26 bytes, array locations from 0 to 5 that is 6 bytes are overwritten and nothing is written at array location after 19. that is array location from 20 onward are blank

and Yes I know that I will have to increase MAX_PDU_SIZE in ble_user_config.h file.
and I have set #define MAX_PDU_SIZE 50
BUT,
why data is being overwritten
Please give me the solution