Part Number: CC2650MODA
Other Parts Discussed in Thread: BLE-STACK, CC2650
Hi experts,
Please let me confirm the certification of CC2650MODA.
- Currently on the product page, the protocol is listed as BLE4.2.
:www.ti.com/.../CC2650MODA - However, BLE-Stack 2.2.3, which can be used with the CC2650, is BLE5.1.
:e2e.ti.com/.../simplelink-bluetooth-sig-certification-update-updated-october-2020 - Also, the datasheet says "2.4-GHz RF Transceiver Compatible With Bluetooth low energy (BLE) 5.1 Specification and IEEE 802.15.4 PHY and MAC".
:www.ti.com/.../cc2650moda.pdf
Q1:From the above information, I understood the following, is it correct?
Although the CC2650MODA is certified as a BLE5.1 product, the protocol and functions used are those of BLE4.2.
Although BLE4.2 functions are sufficient, we would like to confirm whether it can be used in cases where we want to label the product as BLE5.1.
Best regards,
O.H