I am planning to use CC2640R2FYFVR component in my design. Due to size limitation on the PCB, I am unable to use the power inductor of 10uH with 220mA current rating (as used in the launchpad) in my design. So, I am thinking to use 10uH inductor with 120mA current rating. This 120mA rated inductor is of 0402 package, so I can save some space on the PCB.
Is it okay to use the 120mA rated inductor?