Part Number: CC2640R2L
Other Parts Discussed in Thread: CC2640
Hello.
We use CC2640 with a 3.6V lithium battery. In fact, we have power
3.7 V. At temperatures less than -5 degrees CC2640 reboots after
1-3 minutes with error AON_SYSCTL: RESETCTL: RESET_SRC Brown out detect on
VDDS. And after a successful OAD, the CC2640 restarts only at a temperature
above zero.
We put a Schottky diode into the power circuit, and then random
the reboots are gone and the OAD is working fine.
Why is this situation with a 3.6V lithium battery?