This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RB: Can the LED module in syscfg achieve a duty cycle adjustable waveform

Part Number: CC2652RB


Hi team,

Here's an issue from the customer may need your help:

The customer would like to implement "1 Hz, on 200 ms, off 800 ms, and flicker 10 times", but due to the below restrictions, it failed:

  • The LTE module enables blinking of the LED as well as brightness control.
  • The period value of the PWM cannot be set too large (the LED does not work when greater than some value), is there any limitation? Setting pwmPeriod to 1000 works fine, but the LED does not light up when set to 1000000.

Could you help check this case? Thanks.

Best Regards,

Cherry