Other Parts Discussed in Thread: CC2540
Hello All,
After going thru the code, I saw that bonding (bond manager) can not be enabled for master device in the demo codes.
Is there any way to establish a secure connection using the CC2540 USB dongle.
I saw the GAP_Bond command in the Btool but its not able to establish a bond with another device.
The GAP_Bond command always fails with status, 0x06(InvalidEventID) with Btool dump as
-----------------------------------------------------------------------------------------------
[3] : <Rx> - 05:33:44.394
-Type : 0x04 (Event)
-EventCode : 0xFF (HCI_LE_ExtEvent)
-Data Length : 0x05 bytes(s)
Event : 0x060E (Unknown Op Code)
Status : 0x06 (InvalidEventId)
Raw : 06 00 00
Dump(Rx):
04 FF 05 0E 06 06 00 00
Please advise how to enable the Bond Manager for Master role device or use GAP_Bond command or any other way to establish a secure connection.
thanks
-krishan