Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: SYSCONFIG, SIMPLELINK-CC13XX-CC26XX-SDK
Hi,
I'm facing a problem with integrating the timer driver with the BLE stack.
Timer_init();
Timer_Params_init(¶ms);
params.period = 1000000;
params.periodUnits = Timer_PERIOD_US;
params.timerMode = Timer_CONTINUOUS_CALLBACK;
params.timerCallback = timerCallback;
timer0 = Timer_open(CONFIG_TIMER_0, ¶ms);
if (timer0 == NULL) {
/* Failed to initialized timer */
while (1) {}
}
if (Timer_start(timer0) == Timer_STATUS_ERROR) {
/* Failed to start timer */
while (1) {}
}
when I add this timer code to the BLE Stack main, that timer0 instance is getting NULL and its getting failed to initialize when I try to place it anywhere with BLE STACK.