Hello E2E,
In this application report, it was stated that at 2440MHz high Power PA target load impedance is 200 Ohm. Where is this 200 Ohm located in the LAUNCXL-CC1352P-2 schematic?
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
In this application report, it was stated that at 2440MHz high Power PA target load impedance is 200 Ohm. Where is this 200 Ohm located in the LAUNCXL-CC1352P-2 schematic?
Regards,
Carlo
Hi Carlo,
We are in the process of updating this document and the latest recommendation and load impedance is the following:
Regards,
Richard
Hello Richard,
Does it mean that in Tx Mode, if we connect a Network Analyzer after the C58 (47pF) (before the RF Switch) on the of LAUNCXL-CC1352P-2, we should measure a Load in the range of 26+j250 ? Please confirm.
Regards,
Carlo
Hello Richard,
Our customer is using a spectrum analyzer connected to the launchpad reference design and they could never reach 20dBm.They only get17dBm and they're using the same component value as per TI matching recommendation. Will there be an update on these reference design or not and in which document?
Regards,
Carlo
Hi,
Make sure the customer is using the latest version of the SmartRF studio since the power settings have been updated from older versions.
There are no plans to update this design. 20 dBm is achieved on the LaunchPad. Send the layout in gerber format so we can help review the layout.