Hello;
I am trying configure "host_test" project.
There is some note which is below;
"Note: Host Test does not automatically respond to Connection Parameter Update Requests and instead allows the application to specify the response parameters. Responses must manually be sent within 40 seconds of reception of the GAP_LinkParamUpdateRequest event (0x0612) using HCI_LERemoteConnectionParameterRequestReply or HCI_LERemoteConnectionParameterRequestNegativeReply"
How can I configure this project for automatic connection, paswoord of connection?
Best Regards.