Part Number: LP-CC2652RSIP
Dear Team;
Simple peripheral project is loaded to emulation bord. it draws 1.2mA.
How can I decrease power consumption?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-CC2652RSIP
Dear Team;
Simple peripheral project is loaded to emulation bord. it draws 1.2mA.
How can I decrease power consumption?
Best Regards.
Hi,
I'll ask an expert to comment.
In the meantime, make sure to review the following resources https://www.ti.com/lit/swra478
Best regards,
Hi OOMAR,
The current draw observed is indicative of the XDS110 debugger still being connected. You will also need to confirm that POWER_SAVING is defined, and there are several relevant E2E threads you can reference.
Regards,
Ryan
Hello,
As Ryan mentioned, this seems like the debugger is active, please make sure to disable the debugger. Are you observing this power consumption on the LP-CC2652RSIP launchpad? If so, then can you please share your measurement set up? Please ensure that the power measurement methodology matches the procedure shown in the application report shared by Clement. Are you removing all jumpers along the XDS except the GND and 3.3V jumpers? Can you share a picture of the LaunchPad during measurements?
Best Regards,
Jan