Part Number: CC2564C
Other Parts Discussed in Thread: CC2564
WE PROVIDED OUR BOARD WITH THE CC2564C MODULE, REALIZING A 3 WIRE UART INTERFACE WITH ONLY RXD AND TXD SERIAL LINE FROM THE PROCESSOR (ST32F437ZI AND FreeRTOS) TO CC2564 (AND COMMON GROUND).
WE ALSO HAVE PULLED DOWN WITH A 100K RESISTOR PIN A29 (HCI-CTS)
WE WANT TO USE THE TI SUGGESTED STACK FOR ST MICROPROCESSOR FAMILY BUT IT SEEMS REALIZED JUST TO SUPPORT A 4-WIRE UART INTERFACE (HW SOLUTION) THAT IS A H4 PROTOCOL, INDEED WE NEED THE STACK SHOULD BE ABLE TO MANAGE AN H3 PROTOCOL,
SO, HOW WE CAN SET THE STACK TO H5 PROTOCOL FOR OUR HARDWARE WITH A 3-WIRE SOLUTION?
MUST WE ABSOLUTELY INCLUDE BOTH RTS /CTS LINES? WE HOPE WE DON'T HAVE TO CHANGE OUR HARDWARE DESIGN
BEST REGARDS
FABIO ORSINI