Part Number: LAUNCHXL-CC2640R2
Hello,
I have an MSP342 evaluation board and the LAUNCHXL-CC2640R2. The simple central project runs on the MSP board and the simple host project runs on the LAUNCHXL-CC2640R2 board.
I would like to change the name of the BLE device via an HCI command. Unfortunately the name will not be changed. I track the communication with an nRF2 stick.
I use this HCI Command
GAP_UpdateAdvertisingData with opCode 0xFE07
adType, 0x00
dataLen,
advertData
HCI_StatusCodes_t setDeviceName(void)
{
HCI_StatusCodes_t status;
unsigned char pData[8]=
{
0x00,
0x06,
0x05,
0x09,
't',
'e',
's',
't'
};
status = HCI_sendHCICommand( 0xFE07 , pData, 8);
// Return Status
return status;
}
This sends over the UART
0x01 0x07 0xFE 0x08 0x00 0x06 0x05 0x09 0x74 0x65 0x73 0x74
Thanks