This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Power Consumption Mismatch between LAUNCHXL-CC2640R and CC2640R2-5X5 Module

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640

I am developing one module which can sense the analog signals, I2c Signals, Battery Data and transmitt it over the ble characteristics.

In addition it also interfaced with a tactile switch which can bring CC2640 in to power saving mode as well as in the operation mode.

Code Controller

However I tried here attached code in the CC2640R2 LaunchXl Module which is 7*7 module. It is working fine with all the functionality with the low power consumption.

Its power consumption rate is mentioned below.

1) When in Shutdown Mode - ~90uA.

2) When in BLE advertise Mode with LED ON - ~5mA

3) When BLE data transfers with LED ON - ~7mA

when I try to do the same with the CC2640R2 Module which has 5*5 Chip inside it I am facing weird issues. It is going in to the power saving mode i Think. Its power ratings are like

1) When in Shutdown Mode - ~5mA.

2) When in BLE advertise Mode with LED ON - ~7.5mA

3) When BLE data transfers with LED ON - ~9mA

I am sharing my code here, please let me know if I am doing anything wrong here, I am attaching the module link which i am using in my circuit for better understanding.

www.alibaba.com/.../Flexible-Oem-Odm-Option-Cansec-An2640R2Sa_1600228856779.html