Part Number: CC2640R2F
Hi!
We are working with a CC2640R2F on a custom hardware with SDK 4.40.00.10.
Once the MCU gets triggered (red line in graph) the application is communicates with some onboard sensors and sends 5 BLE beacons at an intervall of ~150ms. After that the MCU is shut down again and waits for the next trigger.

When looking at the current consumption (blue line, using the TI XDS110 debug probe) I see a significantly high current once the RF unit is started (yellow circle) but not yet sending.
Is that normal behaviour or is something misconfigured there?
I am trying to reduce the overall consumption per triggered event and this part takes quite a bit of energy.
Thanks for any inputs!
Cheers
JR