This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Tuning the HF Oscillator

Part Number: CC2640R2F

Hi team,

We want to tune the HF Oscillator "6.4 Tuning the HF Oscillator"(swra640.pdf).

We assume that the way to do it is:

CMD_TX_TEST: Transmitter Test Command (23.3.3.1.8 in swcu117.pdf)

MODE_CONF Register (Offset = FB4h) (9.1.1.4 in swcu117.pdf)

Is it correct way?

If it is, could you please tell me the specific method to do it?

If possible, the method without SmartRF studio is better for us.

Best regards,

Yuto

  • Hi Yuto,

    Yes, without SmartRF studio, you'll have to modify the registers directly. I recommend using the rfCarrierWave example and a spectrum analyzer to determine the offset needed (if any). It will take some trial and error, but you just need to enable and modify the cap array using the MODE_CONF Register and make adjustments as needed. 

    Thanks,

    Alexis