Hello,
how much flash/ram space is used by the BL stack from the 352kB flash/32kB RAM or how much memory can be used by the application?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
how much flash/ram space is used by the BL stack from the 352kB flash/32kB RAM or how much memory can be used by the application?
Regards, Holger
Hi Holger,
The answers depend on the Bluetooth features used, the SDK version used, the number of connections, the size of the GATT table, the number of bonds, the toolchain used, etc.
I would recommend you to build the example (simple_peripheral or simple_central) you want with the configuration and toolchain you need to have a better idea.
Best regards,
Hello Clement,
some estimation would help. I don't have tool neither the customer.
Some parts of the BLE stack are stored in ROM?
Regards, Holger
Hi Holger,
On CC2651 devices, the BLEStack is not stored in ROM.
Best regards,