This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: How to fix the XDS110?

Part Number: CC2642R

I have a cc2642r1f development kit, when using Flash Programmer to upgrade the XDS110 firmware, the USB was removed.

So now the computer can't detect it, and Found 0 devices using command: xdsdfu -e

How to fix it?

  • Hi,

    I'll try to find an expert to comment but I am not sure this error is actually recoverable.

    In the meantime, would you happen to have an other LaunchPad? No matter which CCxxxx device this LaunchPad has, you could use the XDS110 from this board. To do so, remove all the jumpers from the top row of both LaunchPads, then use jumper wires to connect the working XDS110 to the CC2642R device.

    Let me know  if you need more details.

    Best regards,

  • Yes, I can only use another xds110 for debugging now.