Other Parts Discussed in Thread: CC2652R, UNIFLASH, CC2650,
Hi TI,
We're having trouble upgrading an image to CC2652R7 via Uart serial.
The original design of our board was to use CC2652R.
We can use sblAppEx from SWRA466 to upgrade FW on CC2652R.
Currently we are using CC2652R7 as the 2nd source on our board.
But it's failed to use sblAppEX to upgrade FW on CC2652R7.
The debug message from the console is below
"Timed out waiting for data header from device.
Failed to read device FLASH size"
Is there need any change on sbltool?
If you have any comment, please let me know.
Thank you.
I have updated BLE image on CC2652R7 success by TI EVB with Uniflash,
And the HCI command seems to run success.
So I believe It's should not be the hardware design issue.
Thanks
Jason.