Part Number: CC1352P
Other Parts Discussed in Thread: CC3200AUDBOOST, CC2642R
Hi,
I wanted to evaluate the range of BT in audio applications and therefore imported the Central Bidirectional Audio and the Peripheral Bidirectional Audio examples. Firstly, this is my SW/HW setup:
Hardware:
- CC1352P-2-LaunchPads
- CC3200AUDBOOST
Software (what I already installed for other examples):
- CC13x2 CC26x2 SDK 5.20.00.52
- CC13x2 CC26x2 SDK 5.40.00.40
- CC13xx CC26xx SDK 6.10.00.29
- SimpleLink Audio Plugin 3.30.00.06
If I try to import either of both example projects, I get following warning:
And if I ignore the warning and continue, when building the project, I get the following compile errors:
The first one is simple to avoid, since I already had this error on other example projects as well. But the rest of it makes me wonder if I have the wrong SDK version dowloaded. I couldn't find any hint on which SDK version this example is based on in the readme file.
Any hints would be appreciated.
Thank you in advance.
Best regards,
Alex