Part Number: CC2652P7
My customer is using CC2652P7 with a Linux host processor. In a test they found that about a half of their boards failed when flashing through ROM bootloader. The CC2652P7 chip on the board does not respond to the 0x55 hand shake.
The customer has tried to switch the CC2652P7 between a good board and a failed board, the problem goes with the board, not the chip.
I have two questions regarding to the ROM bootloader:
1. Does the ROM bootloader use external 48MHz crystal or internal RCOSC?
2. Is there a way to debug the ROM bootloader, like through JTAG? Or other suggestions to debug why the chip is not responding?
Best regards,
Shuyang