Part Number: CC2640
Other Parts Discussed in Thread: CC2650STK
I used the hex file provided by others to burn, but the second burning error is as follows:
>Initiate access to target: COM46 using 2-pin cJTAG.
>Reading Primary MAC address finished.
>Start flash erase ...
>Erase finished successfully.
>Reading file: C:/Users/jun.yang/Desktop/simple_ peripheral_ cc2650stk_ all_ v1.6.0_ rev188.hex.
>Start flash programming ...
>Programming finished successfully.
>Reading Primary MAC address finished.
>Initiate access to target: COM46 using 2-pin cJTAG.
>Debug interface is locked. Aborting action. Only forced mass erase is possible.
>Debug interface is locked. Aborting action. Only forced mass erase is possible.
I did not solve the problem after erasing it, nor did I solve the problem after changing the chip