Hi Teams,
I'm trying to build an HID device with CC2640R2F.
I try to modify the hid_emu_kbd project in simplelink_cc2640r2_sdk_ble_example_pack_1_50_00_62 refer to the code of HOGP-BLE-HID-EXAMPLE for CC2652. The keyboard and the consumer control work fine but the mouse doesn't work.
Here attached the source code, could you help me?
Working tools version based on the followings,
(1) Hardware: Customer Design (the board works fine)
(2) CCS: 10.4.0
(3) SDK: 1_50_00_58
(4) XDCTOOLS: 3_50_03_33_core
(5) TI ARM Compiler: V16.9.4 LTS
Regards,
Jingkun