Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: Launchpad not running custom code

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, UNIFLASH

Hello E2E, 

I am attempting to run a custom code which is based on the simple peripheral project on my cc2650 Launchpad, however I get the following error: "[Program]: Specified Program ( Texas Instruments XDS110 USB Debug Probe_0/Cortex_M3_0 )  does not exist" in the debug configuration tab. How do I fix this in the code for ccs to recognize xds. 

  • Hello Abe,

    Are you still using the LAUNCHXL-CC2650 hardware and can you successfully program the default simple peripheral project?  Are you using the same target configuration (.ccxml) for your custom code?  Can you program the code through a different software solution such as Uniflash or Flash Programmer 2?

    Regards,
    Ryan