This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: BIN file not generated(Post build error)

Part Number: CC2640R2F


Hi all,

     I am working with OAD-off chip project. In my PC the project is building properly and even post build(which generates the BIN file) also happened properly. I have shared my workspace including the project with my colleague. For him, pre-build is happened properly but post-build failed. So, in his laptop we cant able to generate the BIN file for this project. But we are able to debug the project since pre-build happened successfully.

Below is the post-build error log:

makefile:219: recipe for target 'post-build' failed

usage: oad_image_tool [-h] [-v] [-verbose] [-hex1 HEXPATH1] [-bdf BDFILEPATH]

                      [-hex2 [HEXPATH2]] [-k [KEYFILE]] -o OUTPUT

                      ProjType ProjDir BinaryType

oad_image_tool: error: argument BinaryType: invalid int value: 'LED/control_card_v1.0/control_cord_v1.0'

gmake[2]: [post-build] Error 2 (ignored)

Please help us to resolve this issue

Regards,

Aslam