Part Number: LAUNCHXL-CC2650
Hello,
I am using LAUNCHXL-CC2650 with
BLE SDK 2_02_07_06
CCS7.4
Compiler TI v5.2.6
In which I have loaded "Simple BLE peripheral" code to receive data from other ble device.
I have already done modifications in code to receive 200 bytes in one packet (by increasing the PDU size, so problem in that thing)
Other device is sending me 29 packets of 200 bytes in each packet one after one.(5624 bytes in total)
The time taken by my LAUNCHXL-CC2650 to receive this 5624 bytes data is 1 minutes and 49 seconds.
which is very high.
please guide me to solve this issue.