Part Number: CC2640
Other Parts Discussed in Thread: BLE-STACK
Hi Engineers,
I have a customer ask a question about CC2640 and its SDK https://software-dl.ti.com/simplelink/esd/ble_stack_2_x/2.02.07.06/exports/release_notes_BLE_Stack_2_2_7.html
I want to know what does it mean by "Version 2.2.7 of the BLE-Stack is a maintenance update to TI’s existing royalty-free Bluetooth low energy software protocol stack which is certified for Bluetooth specification version 5.1. This release includes support for all core specification version 4.2 Low Energy (LE) features as well as several development kits. This protocol stack update is in addition to support of all major Bluetooth LE core specification version 4.1 features, including support for up to 8 master or slave BLE connections. Please note that no Bluetooth 5 or Bluetooth 5.1 features are supported. " Can this SDK support BLE 5.1 or not? It is confusing to see both answer "is certified for Bluetooth specification version 5.1" and "no Bluetooth 5 or Bluetooth 5.1 features are supported"