Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: reset sensor controller

Part Number: LAUNCHXL-CC1352R1

Hi team,

Here's an issue from the customer may need your help:

SDK: simplelink_cc13xx_cc26xx_sdk_6_10_00_29

On the application side, is there any instructions can reset sensor controller only or power cycle sensor controller only? Thanks.

Best Regards,

Cherry

  • Hi Cherry, 

    The Sensor controller is in the Aux domain(AON_VD) which is always powered when the device is not in shutdown. I didn't find anyway to power cycle the sensor controller only. The AON_VD is reset with a system reset. 

    Regards,
    Sid