Part Number: CC2642R
Hi,
I work on a project which create a factory image of the current running image each time a OAD is performed.
From my understanding of the OAD process, this step does not provide further robustness for my project and can be removed to save space in the external flash.
Reasons why:
- No HMI like a button is available to trigger the revert mechanism in the BIM
- The factory image is always based on the current running image and not a special one loaded from production.
- In case a downloaded image in external flash fails (e.g. crc check), the image in internal flash will be intact and reused.
- In case the process fails of overwriting the internal flash with a validated downloaded image from external flash, the process will continue/start over next time the BIM is running.
Do i miss anything or is it true that for my project I can skip this step?
Best regards,
Christoffer