This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P7: Passcode protection

Part Number: CC2652P7

Hello

I try to protect my device with a passcode i have folow

www.ti.com/.../swru393e.pdf 5.4.4.3 Passcode Entry

The pairing work fin with android but if I unpair. reconect (with ble scanner) and when android request pairing i reply Cancel the connection are axcepted and i can read caracteristique

How i can refus connection or characteristique read/write for no paired device?

uint8_t pairMode                =    GAPBOND_PAIRING_MODE_INITIATE;
uint8_t mitm                    =    true;
uint8_t ioCap                   =    GAPBOND_IO_CAP_DISPLAY_ONLY;
uint8_t bonding                 =    true;
uint8_t secureConnection        =    GAPBOND_SECURE_CONNECTION_ONLY;
uint8_t authenPairingOnly       =    true;
uint8_t autoSyncWL              =    false;
uint8_t eccReGenPolicy          =    0;
uint8_t KeySize                 =    16;
uint8_t removeLRUBond           =    false;
uint8_t KeyDistList             =    GAPBOND_KEYDIST_MENCKEY | GAPBOND_KEYDIST_MIDKEY | GAPBOND_KEYDIST_MSIGN | GAPBOND_KEYDIST_SENCKEY | GAPBOND_KEYDIST_SIDKEY | GAPBOND_KEYDIST_SSIGN;
uint8_t allowDebugKeys          =    false;
uint8_t eraseBondWhileInConn    =    false;

void setBondManagerParameters()
{
    // Set Pairing Mode
    GAPBondMgr_SetParameter(GAPBOND_PAIRING_MODE, sizeof(uint8_t), &pairMode);
    // Set MITM Protection
    GAPBondMgr_SetParameter(GAPBOND_MITM_PROTECTION, sizeof(uint8_t), &mitm);
    // Set IO Capabilities
    GAPBondMgr_SetParameter(GAPBOND_IO_CAPABILITIES, sizeof(uint8_t), &ioCap);
    // Set Bonding
    GAPBondMgr_SetParameter(GAPBOND_BONDING_ENABLED, sizeof(uint8_t), &bonding);
    // Set Secure Connection Usage during Pairing
    GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &secureConnection);
    // Set Authenticated Pairing Only mode
    GAPBondMgr_SetParameter(GAPBOND_AUTHEN_PAIRING_ONLY, sizeof(uint8_t), &authenPairingOnly);
    // Set Auto Whitelist Sync
    GAPBondMgr_SetParameter(GAPBOND_AUTO_SYNC_WL, sizeof(uint8_t), &autoSyncWL);
    // Set ECC Key Regeneration Policy
    GAPBondMgr_SetParameter(GAPBOND_ECCKEY_REGEN_POLICY, sizeof(uint8_t), &eccReGenPolicy);
    // Set Key Size used in pairing
    GAPBondMgr_SetParameter(GAPBOND_KEYSIZE, sizeof(uint8_t), &KeySize);
    // Set LRU Bond Replacement Scheme
    GAPBondMgr_SetParameter(GAPBOND_LRU_BOND_REPLACEMENT, sizeof(uint8_t), &removeLRUBond);
    // Set Key Distribution list for pairing
    GAPBondMgr_SetParameter(GAPBOND_KEY_DIST_LIST, sizeof(uint8_t), &KeyDistList);
    // Set Allow Debug Keys
    GAPBondMgr_SetParameter(GAPBOND_ALLOW_DEBUG_KEYS, sizeof(uint8_t), &allowDebugKeys);
    // Set the Erase bond While in Active Connection Flag
    GAPBondMgr_SetParameter(GAPBOND_ERASE_BOND_IN_CONN, sizeof(uint8_t), &eraseBondWhileInConn);
}