Using the older Beta1.0 SDK I was able to connect directly to my Windows 7 PC through the SPP on a regular bluetooth dongle, and get the accelerometer data through a COM connection. I simply had to add a bluetooth device, wait for the RF2560 to show up, and pair using 0000
Using the newer GA 1.0 SDK, as soon as I try to add the device in windows the pairing screen (where I used to enter the code) flashes very breifly, then the pairing fails.
I've updated my bluetooth drivers and tried both my dongles. If I pair them together (one on battery, one on the programmer) I can get about 30 seconds of serial data, but can't keep a constant connection.