Part Number: CC2651R3SIPA
When I open the system configuration tool from the IDE (as well as the standalone version). Its indicates that there are 4 GPIO pins available (those are Pins 27, 29, 33 and 34). We want to use pin 29 as a GPIO output line, but when I try to select pin 29 in the PinMux Peripheral and Pin Configuration section, out of the 4 pins, Pin 29 is not shown in the dropdown menu and this is preventing us from using that pin. There seems to be no way to get around this issue.