Other Parts Discussed in Thread: CC2570, CC2567, CC2571
I am new to microcontroller so please bare with me. I am learning about microcontrollers because I want to create an ANT+ sensors for fitness equipment. I understand I need to use an MSP430 and an antenna to transmit data to the host device. I also understand that ANT is regulated by Dynastream. However I am confused with the following.
If I look at the RF connectivity page on TI's site http://focus.ti.com/mcu/docs/mcuorphan.tsp?contentId=24576&DCMP=MSP430Wireless&HQS=Other+EM+430wireless#pan Under the personal area network table there are two options for ANT devices. The first is the ANT + Bluetooth which uses the CC2567 transceiver. The second option is the ANT+ device which uses the CC2570 which is a Network Processor.
Q1. What is the difference between a transceiver and a Network Processor?
Q2. Can I use the ANT+ Bluetooth setup in a sensor. For example could I use this in a heart rate monitor and read heart rate on an ANT+ device or a Bluetooth device? Or is this not how the ANT+ Bluetooth configurations works?
Q3. If the answer to Q2 is no is my only option the CC2570?
Thanks,
Jon