Other Parts Discussed in Thread: SYSCONFIG, LAUNCHXL-CC26X2R1, SIMPLELINK-CC13XX-CC26XX-SDK, CC2652R
I'm trying to port a set of power pin that wkae up our custom board from 6.10 to 6.20 simplelink SDK
last rev was using PIN driver that no longer exists on 6.20
```
/********** Wake-up Button pin table **********/
PIN_Config ButtonTableWakeUp[] = {
 CONFIG_CHG | PIN_INPUT_EN | PIN_NOPULL | PINCC26XX_WAKEUP_NEGEDGE,
 CONFIG_WAKE_UP | PIN_INPUT_EN | PIN_NOPULL | PINCC26XX_WAKEUP_NEGEDGE,
 PIN_TERMINATE /* Terminate list */
};
[. . . ]
/// before Board_init() calling
PIN_init(BoardGpioInitTable)
Board_init();
PINCC26XX_setWakeup(ButtonTableWakeUp);
```
I try to reproduce same behaviour in 6.20 SDK
but I didnt fine something similar
I just find a define in simplelink sdk doc called `GPIO_CFG_SHUTDOWN_WAKE_LOW` I tried to setitup but after the call to GPIO_init() done in Board_Init()
```
GPIO_setConfig(WAKE_UP, GPIO_CFG_INPUT | GPIO_CFG_SHUTDOWN_WAKE_LOW);
```
but no results
I didnt find any optional config options in sysconfig tool and I just define the pin as input
stangely syscfg is defining it in `gpioPinConfigs` table as INTERNAL
```
GPIO_CFG_INPUT_INTERNAL | GPIO_CFG_IN_INT_NONE | GPIO_CFG_PULL_NONE_INTERNAL,
```
I've search a bit on forums to find some similar questions but as 6.20 sdk is a bit recent I didn't find any answer ...
thank's for any help