This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK
Hi E2E,
Code Composer Studio (Version 12.0.0.00009) crashes when I flash the multi_role example to the LAUNCHXL-CC26X2R1.
I encountered the problem on a custom Application after a SDK migration to 6.20. But I am able to reproduce the issue with an initial multi_role example (SDK 6.20.00.29).
It is possible to build the project with TI Clang v2.1.0.LTS but when I press "Debug" or just flash to the target CCS crashes and shuts down.
I tried it with the simple_central example and it works.
I also used another clang compiler TI Clang v1.3.1.LTS and it works too.
CCS dmp file for crash with multi_role and clang v2.1.0:
1e173551-5bf5-4c29-8c78-03e533c785ad.zip
Best regards,
Sebastian
Hi Sebastian,
This is a known issue, please refer to this relevant E2E thread: https://e2e.ti.com/f/1/t/1121698
You can download newer versions of TI-CLANG: https://www.ti.com/tool/download/ARM-CGT-CLANG/2.1.2.LTS
Regards,
Ryan